Helpful Features

Recent posts

  • 2aliam1qis6nqbsesiyg

    The Evolution of 3 Phase PDUs

    by Annie Paquette

    Server Technology has a conversation with an in-house expert on three phase power. Read this blog to learn how 3 phase PDUs are evolving.

    Categories: Helpful Features

  • Iavzxbatb2ulc7imngdp

    What is a Vertical PDU? Defined.

    by Annie Paquette

    Server Technology provides this thoughtful blog on the topic of peace – and vertical rack mounted PDUs. What is a vertical PDU? Take a peek here.

    Categories: Helpful Features

  • Qwl8b5dhsvahotm6r0vw

    What is a Data Center PDU? Defined.

    by Annie Paquette

    With a host of PDU types available in the market, understanding what a Data Center PDU does can be confusing. This Server Technology blog clears the air on Data Center PDUs.

    Categories: Helpful Features

  • Llejfkhota6noz9so7cg

    What is a Switched PDU? Defined.

    by Annie Paquette

    With a host of PDU types, understanding what a Switched PDU does can be confusing. This Server Technology blog provides information on what Switched PDUs do.

    Categories: Helpful Features

  • Vgakiz4utc2ex2wi5dzh

    Just the Facts Part 2: Data Center Environmental Monitoring Defined

    by RJ Tee

    In our previous post on intelligent PDUs, we dedicated a blog to defining what it means to be an intelligent PDU. In this blog, we will discuss one of the characteristics of intelligent PDUs in more detail: data center environmental monitoring. Intelligent PDUs provide the support network that gives more rack-based data. In addition to power quality or capacity data, intelligent PDUs can be outfitted with data center environment sensors that collect additional information required for the management of the data center. Besides power, feedback on the operation of the cooling system is of utmost importance, but so is the physical security of the rack itself.

    Categories: Helpful Features

  • Ybnany2qvdmlmw3cwdsw

    Just the Facts Part 1: Intelligent PDUs Defined

    by RJ Tee

    intelligent PDU, IP Power Strip, network pdu

    Categories: Helpful Features

  • 5dtmcnbstqsxfwnshjzm

    Then, What is a Switched PDU?

    by Kayla Poole

    In our previous post “So, What Is an Intelligent PDU?” we provided some clarification to what can be thought of as a broad a category of products, all of which have a network connection in common. An intelligent PDU is a basic PDU with a network connection. And like most general categories, there are subcategories that bear some discussion. As we defined it in the last post, an intelligent PDU does two things: first, the network connection provides data feedback on the operation of the unit; second, the network connection provides the ability to control the operation of the unit remotely. From these two features come the two major subcategories in the intelligent PDU world: ‘smart’ for data feedback, and ‘switched’ for command and control.

    Categories: Helpful Features

  • Uqegaxys0oc5dbb21eoa

    So, What Is an Intelligent PDU?

    by RJ Tee

    The term ‘intelligent PDU’ has become so ubiquitous, the definition is no longer clear. Not surprising, “What is an intelligent PDU?” is one of the most common questions we get from our readers. Terms like ‘network power strip’ and ‘IP power strip’ get bandied about, but they somehow fail to capture the essence of choosing and using an intelligent unit. We thought we would take a moment to clear the air about the term, and in doing so, we hope to set the record straight about this class of rack power strips. It is important to think of them as a category or family, if you will, rather than a specific kind of PDU.

    Categories: Helpful Features

  • Fxbuxky8sbs0piuktmx7

    ZTP = PDQ

    by RJ Tee

    If there was ever a situation where practice doesn’t necessarily make perfect, this is it: setting up a PDU manually – without ZTP. As you can see in our new white paper, Server Technology is in the business of making provisioning our power distribution units simpler for you.

    Categories: Helpful Features

  • Pnwkcfs6tsockvsh4uvw

    Top Reasons to Use Switched PDUs in Your Data Center

    by Josh Schaap

    It’s not easy trying to decide which type of rack PDU to purchase for your data center. As we explained in a recent article, the decision ultimately comes down to your data center’s unique needs. Your appetite for risk, facility budget, and operating preferences will all play a big part in determining what type of rack PDU you should be using. In this article, we will focus on the switched PDU, which is a smart PDU that will let you toggle power on and off, on a per outlet bases, from a remote location. A switched PDU also allows you to centralize the management functions of your PDU.

    Categories: Helpful Features

  • 7r5lundsuwcxv6yr0lnx

    Rack PDUs: Making the Choices less of a Challenge

    by RJ Tee

    While in previous blogs we’ve talked about the advantages of customization and having so many PDU options to choose from, now might be a good time to keep it simple. Server Technology is in the business of meeting complex power needs for every customer’s equipment and data demands. But we would be remiss if we didn’t address those needs in the simplest and most straightforward way possible.

    Categories: Helpful Features

  • U8raucfwqgswjyqqi77x

    What does a Rack PDU do again?

    by RJ Tee

    On the surface, it is an amazingly simple question. Everyone knows what a rack PDU is, don’t they? In one of the few industry blogs to reference the movie Gremlins, we attempted to answer the question in the context of the acronym-laden industry we work in. Power Distribution Unit. In this blog we are going to move beyond semantics and talk more about the doing side of a PDU. Our friends will point out that a power strip is just the same thing: a device that has outlets, a cord, and maybe a little surge protection thrown in. To channel my inner Elf, “Say power strip ONE MORE TIME!”

    Categories: Helpful Features

  • Ps52qdumqg2u0rbc5b2y

    The Advantages of an Uncluttered Rack, Part II

    by RJ Tee

    As mentioned in our previous post on Alternating Phase rack PDUs, many of us at Server Technology (including myself) like to talk about the benefits of our approach to handling three-phase power distribution within the rack. While the subject of three phase is de rigueur in the fashionable world of high density, there is a lot to talk about above and beyond the distribution of large amounts of power in a very small footprint.

    Categories: Helpful Features

  • Co5syuvsoy3zkorczei1

    The Advantages of an Uncluttered Rack, Part I

    by RJ Tee

    Alternating phase power distribution technology from Server Tech is one of my favorite subjects. It has benefits that extend well beyond the electrical distribution world. In fact, it is one of the few power products whose secondary benefits meet and sometimes exceed the fundamental purpose of a three-phase distribution product. I discussed it in a previous post. Server Tech’s Alternating Phase PDUs may well set the new standard for the phrase, “the gift that keeps on giving.”

    Categories: Helpful Features

  • Ytevhanqumueddeh3rk0

    On the Benefits of Alternating Phase

    by RJ Tee

    We’ve extolled the virtues of single phase 60A power distribution to the rack. But there are still may situations in which a three phase deployment is required to power the needs of racks that consume 12kW or more. In other words, situations that begin with ‘high’ and end with ‘density.’

    Categories: Helpful Features

  • Edqhhlwqrlaongc2rv8h

    The Rack PDU’s Role in Battling Cyber Threats

    by RJ Tee

    One of the ongoing issues facing data center managers is cybersecurity, and the rack PDU may play a surprising role in the protection of the IT systems housed within the mission critical facility. While threats of intrusion are as old as the IMSAI 8080 from the movie WarGames, the intelligent power strip is a surprising new actor in the ongoing security battle.

    Categories: Helpful Features

  • 5r4qyjjxq11hmiqtqqns

    HDOT Family Welcomes Per Outlet Power Sensing PDUs

    by RJ Tee

    Just in case you didn't know, our award winning HDOT PDUs contain embedded Per Outlet Power Sensing (POPS) with device-level power monitoring, making this the most innovative product line yet. Every data center should seriously consider using HDOT PDUs — with +/- 1 percent billable-grade accuracy — to drive efficiencies, maximize uptime and slash operating costs.

    Categories: Helpful Features

  • 26hbjdinqugjbudtwtdo

    Picking the Right Rack Mount PDU For Your Data Center

    by RJ Tee

    Decisions, decisions. We often stress over relatively easy decisions more than we reasonably should. One decision that shouldn’t be all that difficult – once you’re armed with the proper knowledge – revolves around which type of rack mount PDU you’ll need to help power your data center for the foreseeable future. When picking a rack mount PDU for your data center, pinpointing your exact needs before shopping will save you a lot of time and energy in the long run. Perhaps density is your primary concern. Or maybe uptime is on the top of your checklist, along with capacity planning. That’s where Server Technology comes in. We offer smart, switched and other intelligent rack PDU options ranging from ready-made units with super-fast shipping to PDUs precisely customized to meet your every need.

    Categories: Helpful Features

  • Ttln262zrfaxindr4hdb

    Top Tools For Data Center Environmental Monitoring

    by RJ Tee

    There’s an old proverb that goes, “Trust, but verify.” This sentiment is particularly apt for data center management, where it’s vital to track every metric you can get your hands on. The need for better environmental monitoring capabilities is increasing due to increasing compute, network, and storage densities and increasing operating temperatures in the data center. Thus, keeping close watch over environmental activity in your data center, particularly when it comes to temperature, and humidity in the rack are critical to prevent disasters if left unchecked. So, what is the best way to get four or more data center environmental monitoring points in your cabinets? Sounds like a complicated question, but the answer is simple: Server Technology Intelligent PDUs are enabled right out of the box with the abilities to attach environmental probes that can precisely detail environmental conditions in your data center equipment cabinets. This information is most reliable when measured external to the devices in the cabinet.

    Categories: Helpful Features

  • 3jhsivtpqsmhtfm11hgm

    Help Your Data Center's Tenants Save on Power

    by RJ Tee

    Think about how hard it is trying to get your kids to turn off the lights when they’re not using them. Why don’t they listen? It’s because they don’t pay the bill; and usually, they don’t listen until you start asking them to chip in on the bill. The same problem exists in multi-tenant data centers, where tenants often have little incentives to reduce their energy usage. There is often a big divide between the expectations of tenants who pay premium rates for data center space, and building operators who must deal with exorbitantly high utility bills. Further, mulit-tenant data centers are some of the most egregious environmental offenders due to how much power they consume on a monthly basis.

    Categories: Helpful Features

  • Uokokudetx2rbq3wemtc

    Data Center Consolidation: A Great Way To Reduce Your Carbon Footprint

    by Josh Schaap

    Data Center Consolidation: A great way to reduce your carbon footprint.

    Categories: Helpful Features